cancel
Showing results for 
Search instead for 
Did you mean: 

Download of latest STM32Cube MCU Package examples for STM32H7 (en.stm32cubeh7_v_1-3-1.zip) is empty / corrupted / only 5Kb

SWood.8
Associate III

Whereas selecting v1.3.0 downloads the full ~400Mb file. Anyone else having this problem ?

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Imen.D
ST Employee

Hello,

Thanks for highlighting this issue. We are working to resolve this.

Kind Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Imen.D
ST Employee

Hello @SWood.8​ ,

This issue is fixed now and you can download the patch release v1.3.1.

Kind Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Great : ) will do

It still doesn't show up in STM32CubeMX's "Check for Updates" list for me. Or maybe minor updates are not being listed there?

redmig
Associate III

This is the situation today:

en.stm32cubeh7.zip --> v1.3.0 --> OK (394 MB)

en.stm32cubeh7_v_1-3-1 --> v1.3.1 --> CORRUPTED FILE - NOT OK! (4.93KB)

en.patch_cubeh7.zip --> v1.3.2 --> OK (1.14MB)

Question is: can we skip v1.3.1 and use directly 1.3.2?

Thanks

Imen.D
ST Employee

Hello,

You should use the new patch of STM32CubeH7 V1.3.2, which englobe new fix of UID_BASE definition to the CMSIS STM32H7xx include files and also the fix of LwIP and mbedTLS applications (added in the v1.3.1 patch) 

The patch v1.3.1 will be removed from the ST web site.

Kind Regards,

Imen.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen