STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SIM7600SAH question ?

Dear Members,I tried to send SMS with SIM7600SAH, the code was working but now it's giving me intermittent result...The code//Clear buffer HAL_UART_Transmit_IT(&huart1,(uint8_t*)&aTxBuffer4, sizeof(aTxBuffer4)); HAL_Delay(5); HAL_UART_Transmit_IT(...

use an exsiting project

hi ST Community,I have a problem with my project:so I want to use an exsiting project in the repository (STM32Cube), I enabled the QSPI in stm32f4xx_hal_conf.h then I create a new file called stm32f4xx_hal_qspi.c and I copied the contents of the sam...

0690X000009YiR5QAK.png
idrissmc by Associate III
  • 918 Views
  • 2 replies
  • 0 kudos

Urgent help on USB HID Combined Mouse and Keyboard

Hello All,I have successfully Combined Mouse and Keyboard as a USB device by modifying the USB HID Mouse example and my PC can recognize them. However, I can easily detect the mouse movement and can't detect the Keyboard. By using Bus Hound I could s...

HHass by Associate
  • 3269 Views
  • 3 replies
  • 0 kudos