STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to configure WM8994 codec on the STM32429I-EVAL1 board to read data from 2 digital microphones and output audio on headphones?

I'm trying to catch audio data from 2 digital microphones and pass it to the STM32F4 MCU using AIF1 (Slot 1) of the WM8994 and SAI interface. Also my goal is to output recorded audio data (after some processing of course) using the same codec (STM32 ...

VBila by Associate
  • 1401 Views
  • 0 replies
  • 0 kudos

Problem Occurs When LWIP Continuous Sending Data

Hi, I occur a problem when continuously sending data. I'm working with LwIP_HTTP_Server_socket_RTOS example project in STM32Cube_FW_H7_V1.5.0. (path as STM32Cube_FW_H7_V1.5.0\Projects\STM32H743I-EVAL\Applications\LwIP\LwIP_HTTP_Server_Socket_RTOS). ...

bsahan by Associate II
  • 1148 Views
  • 0 replies
  • 0 kudos

STM32H7 Nucleo board - Ethernet PPS output

Can anyone provide sample code for Ethernet PPS output signal generation?I use Nucleo board, pin PB5 (CN7 connector).I use 43 value for sub second increment registerMy PPS settings: ETH->MACPPSIR = 50000000 - 1;//PPS interval register (1 tick - 20ns...

Andrew1 by Associate II
  • 1073 Views
  • 0 replies
  • 0 kudos

usb device vcp won't give any life on PC

I'm creatring an application on a STM32F412RG. Because I'v to build a lib that integrates in a bigger buid I have to use the standard peripheral lib instead of being able to use CubeMX unfortunately.I'm alreadys truggling for more than a week with ge...

SMaes.3 by Associate
  • 772 Views
  • 0 replies
  • 0 kudos

Can any STM32's operate USB without HSE?

Hi all,I know the older generations of STM32s cant use USB without the use of an external osc.Has this changed at all with the newer L4, F4, G4, etc micros?Have the HSI's improved enough?Thanks in advance.

mwp by Senior
  • 1239 Views
  • 2 replies
  • 0 kudos

LL drivers UART RXNE interrupt not working.

Hi !I am writing a code that uses the UART1 and I would like to work on RX interrupt to handle incoming strings.To start with it, I wrote a code that simply initialise the UART and send a character once the RX Interrupt is fired:#ifndef HSE_VALUE #de...

simo zz by Senior II
  • 968 Views
  • 0 replies
  • 0 kudos

Resolved! using cdc vcp with adc in dma Mode

Posted on December 17, 2017 at 20:58Hello,i am trying to send data from the adc over the usb otg fs as virtual com port to my pc where i receive the data with a terminal program(HTerm).Using the ADC in 8bit Mode works perfectly. The settings are the...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.