STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Overrun error is frequently occured on STM32F415 even on a highest interrupt priority for USART1

Hello, ST experts​STM32F415 runs at 168MHz speed on custom board. And UART1 is used between MCU and a peripheral. The UART baudrate is 460800bps. And UART1 global interrupt is the highest priority interrupt except Non maskable interrupt and Hard Fau...

Yang Yang by Associate III
  • 2944 Views
  • 5 replies
  • 0 kudos

How to make several I2C (slave) addresses in STM32.

Hello,I am trying to connect RaspberryPi (master) with STM32 (slave) via I2C. STM has to "simulate" several devices (exactly 10) on the I2C bus. The problem is that I can set max 2 addresses (at least in Cube - HAL libraries). Ideally it would be lik...

SSoko by Associate II
  • 5278 Views
  • 5 replies
  • 0 kudos

Where is the source code for the NUCLEO-F767ZI ?

I am not able to find the source code for the example provided with this board.When hitting the USR button, it will blink consecutively the three on-board USR leds.I have downloaded the en.STM32Cube_FW_F7_V1.15.0 and en.stm32cubef7 archives but none ...

Philippe by Associate II
  • 1600 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.