STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 ISP-IQTune Port Detection Issue with IMX335 on STM32N657X0H3Q

大家好!问题是这样的: 我正在尝试使用 STM32 ISP-IQTune 应用程序通过 STM32N657X0H3Q 板读取 PC 上的 IMX335 相机数据。但是,IQTune 无法检测到任何可用的 COM 端口。这是我的设置:硬件:板:STM32N657X0H3Q相机:IMX335(MB1854B模块,根据文档提供原生支持)。固件:已从 STM32N6 固件包中刷新 DCMIPP_ContinuousMode 示例。连接:已将板上的两个 USB 端口连接到 PC(USB-C 电缆)。开发板...

陶铸 by Associate II
  • 1942 Views
  • 5 replies
  • 0 kudos

FreeRTOS Tick Speed

Good evening,  I need freeRTOS tick speed to be greater than 1kHz, I tried to change the configTICK_RATE_HZ parameter but get a divby0 error which I can't fix. Is there a way garanteed way to achieve what im looking for? Thx in advance 

Jack_DB by Associate II
  • 444 Views
  • 2 replies
  • 1 kudos

Resolved! I2C Slave sends stale data to Master

Hello! This is the first time I'm using an STM32L0 (...11F4Ux) and also the first time I've tried implementing an I2C IRQ Handler. The code snippet mostly works, but there's a bug in which a READ commands sends data from the previously requested regi...

FP-AUD-AEC1 Hard Fault on STM32WB55REV

Hey everyone,I'm currently trying to integrate the STM32 FP-AUD-AEC-1 software package in a multithreaded environment (ThreadX) on an STM32wb55rev7 mcu chip. Library compiles and runs but eventually hard faults during thread initializations. Any advi...

coop6 by Associate
  • 494 Views
  • 2 replies
  • 0 kudos

SDRAM FMC with STM32H7

Hi everyone, my custom board previously had an STM32F746BGT6. Since we were looking for a microcontroller with a graphics accelerator, we opted for the STM32H743BIT6 (which is pin-to-pin compatible). All the peripherals work, but I'm having trouble i...

Giovanni3 by Associate III
  • 1434 Views
  • 10 replies
  • 0 kudos

Static DFU Serial Number on STM32F723xx

There have been previous posts about determining how the DFU serial number is formed from the 96-bit Unique ID.  However, when using the ROM bootloader for the STM32F723xx MCU I don't see unique serial numbers at all.  I am always seeing the same DFU...

jwj by Associate
  • 574 Views
  • 2 replies
  • 0 kudos