STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HAL_PWREx_EnableWakeUpPin for STM32H743

Dear all,In hal driver datasheet, the funcion HAL_PWREx_EnableWakeUpPin is defined like this : void HAL_PWREx_EnableWakeUpPin (PWREx_WakeupPinTypeDef * sPinParams)In stm32h7xx_hal_pwr.c from STM32Cube FW_H7 V1.5.0 library is defined like this : ...

Problems reading register from I2C sensor using HAL_I2C

Hi guys ! I’m in a bit of a pickle so I finally decided to ask ..I’m using a Dragino sensor node based on STM32. I need to change the default software to be able to read an I2C pressure WNK sensor. I know the sensor’s address is 0x6D. I also know tha...

NDrag by Associate II
  • 927 Views
  • 2 replies
  • 0 kudos

Sir I want to use STM32-AUDIO100A library for my STM32 Nucleo F401RE board but I am not getting the way to use it. If you can provide me any example to use the STM32-AUDIO100A library then it will be a great help for me.

Sir I want to analysis the audio characteristics for my project using I2S protocol so please recommend me the right board for it and please provide me the proper resources for it.

SMitt1 by Associate
  • 942 Views
  • 0 replies
  • 0 kudos

HAL_SMARTCARD_Receive returns HAL_TIMEOUT.

Well, I use STM32 Nucleo F429Zi and Stm32 Cube IDE v. 1.0.2. I connected SmartCard and STM32 correctly (my oscilloscope shows rigth values of RST, IO and CLK) but in code i see zero filled buffer each SET/RESET iteration where ATR should be. Here's s...

SMac by Associate II
  • 973 Views
  • 0 replies
  • 0 kudos

Nucleo L152 HAL_I2C_Master_Transmit_IT problem

Hi all,i tested two method of I2C transmit and resulted as follow.Method 1 : HAL_I2C_Master_Transmit_DMA(&hi2c1, 0x4E, &Data_M[0], 4); Nothing come out at the logic analyserMethod 2 : HAL_I2C_Master_Transmit(&hi2c1, 0x4E, &Data_M[0], 4,1000); Data co...

0690X00000ARVHOQA5.jpg 0690X00000ARVHiQAP.jpg
pchun by Associate
  • 918 Views
  • 0 replies
  • 0 kudos

Resolved! After LL_I2C_TransmitData8 the TXE flag keeps 0

I'm using STM32F103RBT6 to connetc to a OLED with I2C1.The init code is as below.static void MX_I2C1_Init(void) {   /* USER CODE BEGIN I2C1_Init 0 */   /* USER CODE END I2C1_Init 0 */   LL_I2C_InitTypeDef I2C_InitStruct = {0};   LL_GPIO_Init...

DDong.0 by Associate II
  • 1853 Views
  • 1 replies
  • 1 kudos

USB DFU Issues - DFU Clock Recovery System

Hi there,We are designing in the STM32H753 and would like to use the factory DFU bootloader. We are able to use the bootloader on the H743 nucleo board, but on our PCB it fails to complete any actions giving a "connection to the target" lost error in...

TScot by Associate
  • 977 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.