STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Could someone please carefully explain or show a Write Memory Command example (using USART)? (Ref. AN3155, pages 18 - 21) The main confusion is what to send after 'Byte 8' , below I try to show an example of writing 0x42424242 to 0x200001a0 (in RAM).

Sent: 0x7F // Test PatternReceived: 0x79 // ACKSent byte 1: 0x31    // WRITE commandSent byte 2: 0xCE // WRITE command complementReceived:   0x79 // ACK   Sent byte 3: 0x20   ...

SKitt by Associate II
  • 2915 Views
  • 7 replies
  • 0 kudos

Bootloader and USB detection on windows

Hello,I m a little bit lost. I want to create a midi board which plug on computer via USB port.I wanted to ask this question on stm32duino forum but seems to be down for a long time (I planned to user stm32duino to program). Can I ask question here ...

BAure by Associate II
  • 2335 Views
  • 4 replies
  • 0 kudos

Incorrect readings ADC12_COMMON register

Tests STM Studio Ide and microcontroller from the stm32G474 series. The debugger incorrectly reads the ADC12_COMMON register values. When I read the registers into the variable, everything is ok, it's correctly set. I attach a photo.

mJar by Associate
  • 1958 Views
  • 4 replies
  • 1 kudos

FatFS + SD + f_utime = not setting the timestamp on the previous ".." and current "." directory name in the subdirectory when listed in the command prompt .

After using FatFS to create and time-stamp a directory on an SD card, when viewing the results using the command prompt to list the contents of the directory, the first two files shown are always the '.' and '..' entries. These are not getting time-s...

Resolved! Next error in stm32f4xx_ll_usb.c?

In function USB_EP0_OutStart is: if (dma == 1U) {   USBx_OUTEP(0U)->DOEPDMA = (uint32_t)psetup;   /* EP enable */   USBx_OUTEP(0U)->DOEPCTL |= USB_OTG_DOEPCTL_EPENA | USB_OTG_DOEPCTL_USBAEP; }In my opinion enabling endpoint should be out of DMA condi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.