STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Blink led with 2 multithread, sinch problems

Hi all,I'm starting a new app with two threads.If I run as debug step by step it works great.But if I run free on the board, the second thread not works good (it doesn't blink the required times).I've use CubeMX for the code generation with Time Base...

0690X000008AUj4QAG.png

STM32F769 Disco LWIP DHCP Can not get IP address

Hello,I am currently working on the project with STM32F769 Disco and i want to use ethernet (with RTOS).I configured all the options in CubeMX and I have a problem with getting IP address using DHCP.The problem is that I get the IP address only in 50...

qqAnton by Senior
  • 2994 Views
  • 6 replies
  • 0 kudos

Resolved! Gaps when playing audio file with DAC

I'm trying to play a sound file with raw PCM data using the DAC:uint8_t buffer[16384]; // 4-aligned uint8_t *bufptr[2] = {buffer, buffer + sizeof(buffer) / 2}; int curr_buffer = 0; volatile int audio_dma_half_complete = 0;   f_read(fh, buffer, sizeo...

0690X000008ASjiQAG.png

How to get UART data properly?

Hi, I'm using stm32f401RE.I set UART functions by using CubeMX and I'm trying to get data from UART and distinguish them.Here is the code.uint8_t RxBuffer[8]; HAL_UART_Receive_IT(&huart2, (uint8_t*)RxBuffer,sizeof(RxBuffer));​ // Writed in while loop...

dlee.0 by Associate II
  • 746 Views
  • 2 replies
  • 0 kudos

Ethernet receive stability using TCP

Receiving TCP stream that spans two packets fails after several seconds. Pings still work. The STM32F7 replies to the receive stream with duplicate ACK'sThe TCP stream does not recover.Ethernet Receive Logic Review using STM32Cube_FW_H7_V1.3.2/Proj...