STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LWIP&FreeRTOS without MPU&Cache

Hi all,i have to port an application using LWIP and FreeRTOS from stm32f429/407 to stm32h743 (EVAL2 board). In the example from Cube Repository (STM32Cube_FW_H7_V1.5.0\Projects\STM32H743I-EVAL\Applications\LwIP\LwIP_HTTP_Server_Socket_RTOS\), there i...

ECiav by Associate II
  • 1380 Views
  • 1 replies
  • 0 kudos

STM32F777T6 BOOTLOADER EXAMPLE

Hi All,I am using the STM32F777T6 board with Attollic studio along with STM32Cube MCU package version 1.9.7 (My set up in Linux base).I need boot loader example for STM32F777T6 board. Please share the example. I have used other reference examples but...

Hi All!!. I am facing this weird issue with my STM32F411RE series eval board. And i am getting HardFault on UART initialize.

I enable freeRTOS (CMSIS_v2) middleware , trying to play around with threads. One of the thread has simple UART transmit function sending some sample message. As soon as the debugger reaches UART_Transmit functions it goes to HardFaultHandler and thr...

ambinabhi by Associate II
  • 1665 Views
  • 4 replies
  • 0 kudos

STMH7 SPI slave DMA question

for the function HAL_SPI_TransmitReceive_DMA, It says in the documentation that it is non-blocking, in that case in slave mode would that mean it won't start until the master started the spi clock? Thanks

STM32h747-DISCO Ethernet Init Failure

Hi, allI just got to learn to use stm32 and got a STM32h747-DISCO kitThere is no Examples of Lwip, so I build a project with cubeMXAnd it run in infinite_loop in LAN8742_Init,      /* Get the device address from special mode register */       for(add...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.