STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How using HRTIM as push-pull for the STM32G474

Hi,Is there anywhere an example how we can use the HRTIM in push-pull mode and how to start the timer?I had use the following instruction, but the outputs are always low.HAL_HRTIM_WaveformOutputStart(&hhrtim1, HRTIM_OUTPUT_TE1 | HRTIM_OUTPUT_TE2);   ...

OGhis by Senior
  • 3114 Views
  • 4 replies
  • 1 kudos

F446ZE - Keyboard and mouse USB host!

Hey,Doing some research on STM32F446ZE and i have successfully made both USB ports to work with a HID device. HS as a FS with my own USB female, and ofcourse with the onboard usb-in.My goal is to use the board as a host for both keyboard and mouse si...

jomoi by Associate II
  • 1745 Views
  • 3 replies
  • 1 kudos

Multi-channel SDADC on STM32F373 using HAL

This question was asked but it is now closed , so i want to ask again If some one can share code of how to do sdadc3 for multichannel viaDMA |ISR | interrupts | preferred DMAAll code example shows how to work with single channel.The reason ...

EA50 by Associate
  • 1351 Views
  • 1 replies
  • 0 kudos