2019-01-11 1:00 PM
I have a question on initialization in a custom booloader and application code.
Usually initialization of a bootloader is as follows:
When jumping to application (after disabling interrupts) I usually employ all of the above, re-initializing clocks and peripherals again and enabling interrupts. I also modify SCB->VTOR in a SystemInit() to set it to 0x08008000.
The question is - since all registers are kept intact (are they?) after jump, would it be legal and advisable to do the following in application initialization:
Of coarse, all skipped steps should be conditionally employed in debugging by USE_DEBUG option.
Is anything wrong with this approach?
Would it be safer just to use all the routines in both bootloader and application?
Thank you,
Gennady