STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is there an example of using the stm32f7xx_hal_eth driver to send raw ethernet frames without using lwip ?

Hello community,Can someone please provide me with an example of using the stm32f7xx_hal_eth driver to send raw ethernet frames without using lwip ?I am trying to send raw ethernet frames with an STM32F746G-Disco but can't figure out what APIs to use...

khaaal by Associate II
  • 1208 Views
  • 1 replies
  • 0 kudos

Resolved! USB CDC Power request

Does the STM USB CDC driver support power negotiation? If so please could someone point me to where I configure a request for more than the default 100mA.I'm using STM32F407 and CDC is working nicely but the computer only shows that 100mA is reques...

PMath.4 by Senior III
  • 1410 Views
  • 2 replies
  • 1 kudos

ST official example code (stm32cube_fw_l4_v1140->32L496GDISCOVERY-> QSPI_MemoryMapped )has optimization "Instruction scheduling" bug!

Official board: STM32L496G-Discovery board(MB1261B)IAR version: 8.32.3.2028Example code : QSPI_MemoryMapped (location: stm32cube_fw_l4_v1140\STM32Cube_FW_L4_V1.14.0\Projects\32L496GDISCOVERY\Examples\QSPI\QSPI_MemoryMapped)​The demo code run the WRO...

adong by Associate
  • 757 Views
  • 1 replies
  • 1 kudos

UART RX overrun at specific condition

Hello again!I've got (another) weird problem working with both H743 and H750 (rev X and rev V). Here is my setup:SYSCLK = 400 MHz (from HSI RC)UART8 = 100 MHz, Async mode, only RX/TX, 19200-8-1-NUSART1 = 100 MHz, Async mode, only RX/TX, 19200-8-1-NUS...

Peaga by Senior
  • 875 Views
  • 2 replies
  • 0 kudos

FAT SD card works, FAT32 doesn´t. Why?

Hello everybody,i am using a STM32F401RE nucleo board and have implemented USB as mass storage device and a SD card with SDIO 1 bit mode.When I am using 2 GB SD card with FAT. Everything works like a charm. Windows shows me the SD card after 1 second...

JCorn.2 by Associate II
  • 1448 Views
  • 3 replies
  • 0 kudos

STM32F303 USB VCP device not showing up - windows 10

I'm having issues getting USB to work on STM32F303RE. The device doesn't show on windows machine. I'm using 24 MHz 10ppm external xtal. I generated initialisation code for keil with cubemx (using STM32Cube FW_F3 V1.10.0) with just USB enabled and it ...

GPavl by Associate
  • 1078 Views
  • 2 replies
  • 0 kudos

STM32F4 ==> LwIP_DNS

Hello sir, I want to use DNS for my project, but it is not easy, I need your help. From now, I succeed to port IP address. but it is failed to use DNS. I set the DNS on the STMC32CUBEMX and checked in the file <<Lwipopts.h>> =================Procedur...