STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429ZIT6 reports wrong bootloader version 3.1 (only 7.x and 9.x should be possible according to AN2606 datasheet)

I'm trying to make communication with bootloader according to AN2606 and AN3155 datasheets.This small python program sends the Get command (0x00 0xFF) to get available commands and the bootloader version: (starts with 0x7f to select UART bootloader f...

dual Micro SD in one Mass Storage Device

hii need help to have dual Micro SD in one Mass Storage Device in H743 for see two micro sd in pc from one usbproject use two sdio 1 & 2 , devise fs and mass storageit work correct for every micro sd separately but not work together in code last init...

MacLaren by Associate III
  • 1952 Views
  • 4 replies
  • 0 kudos

Resolved! VCONN_SUPPORT

I would like to enable VCONN based on STM32CubeExpansion_USBPD_F0_V2.1.0.I found CMACRO "_VCONN_SUPPORT", but I encountered complile errors below if I used _VCONN_SUPPORT.compiling usbpd_dpm_core.c...../../../../../../Middlewares/ST/STM32_USBPD_Libra...