STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F07 - IAP question, jumping from base 0x08000000 to Application offset. Interrupts not working.

Hi,​I’ve sectioned the STM32G071 into 2 sections with the IAP portion booting up as per default 0x0800000. I’ve also downloaded @ 0x0800A000 the main application code that I would like to run.​During boot, the IAP code executes first and it runs fine...

Dng.14 by Associate
  • 552 Views
  • 0 replies
  • 0 kudos

Regarding Dual Boot into Dual Bank for STM32F767, I see contradictory information. Please clarify how to achieve Dual Boot with F767 to correct bank after power-down cycle.

The attached README.TXT document is an example of contradiction and mistake that has cost me days of wasted time. Following the original instructions, the project does not work. With the changes I finally made (see txt file), now it works. Please ...

design23 by Associate II
  • 540 Views
  • 0 replies
  • 0 kudos

Touch Sensing example code not found

Hi, I was searching for example code for Touch Sensing for STM32L476RG but was unable to find it in the example package STMCubeL4. All I found was a library for touch sensing, but the link attached says that there is an example code for touch sensing...

STM32F767VIT6: SAI1 USB issue

I'm working on a board where SAI1 is wired to a DAC. I've had it working using HAL calls, from a wavetable in RAM. But it needs to play back audio from USB. I tried various approaches; no luck. I was pointed at:STM32Cube_FW_F7_V1.15.0\Projects\STM327...

I'm trying to resolve some ambiguity related to write-while-read of flash within the STM32L4R5ZI. If someone can straighten me out I'd appreciate it.

The FlashErase example project in the STM32Cube_FW_L4 here:D:\STMicro\STM32Cube_FW_L4_V1.13.0\Projects\NUCLEO-L4R5ZI\Examples\FLASH\FLASH_EraseProgram\Src seems to imply that it's possible to erase and write to the same bank of flash that you are exe...

Rvon by Associate
  • 799 Views
  • 3 replies
  • 0 kudos

Resolved! Adding UART to existing project

Hello,I have donwloaded the STM32CUBE FW pack for F1 modules.I tested 2 of them: a UART_PRINTF example and a PWR example, for the F100 Discovery board.Both examples work well, and I want to add UART capability to the PWR example.How does one do it?I ...

ISeed by Senior
  • 760 Views
  • 2 replies
  • 0 kudos