STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Hi, I'm using stm32L073Rz , need to know how to configure it as a usb memory device, no demo examples are available for usb memory stick for this chip , i used cubemx to generate code for usb memory class and ran it.

It does not work , it gets detected as unknown device,what am i missing , should i add something more to cube mx generated code. Thanks.

svii by Associate III
  • 725 Views
  • 3 replies
  • 0 kudos

stm32l476 disc uart DMA not working

#include "main.h"#include "uartDma.h"UART_HandleTypeDef huart2;DMA_HandleTypeDef hdma_usart2_tx;void uartStart(void){ MX_DMA_Init(); MX_USART2_UART_Init(); uint8_t pData[] = "This is Polling\r\n"; uint8_t pdata[] = "This is Dma\r\n"; HAL_UART_Tran...

Jagath by Associate II
  • 472 Views
  • 0 replies
  • 0 kudos

STM32F401 USB remote wakeup does not work

Environment:STM32F401RCUSB HID device, Full speedfreeRTOSProblem:Device can send/receive data to/from host and can be put in suspend state and resume from suspend state.However, the remote wake-up function never worksCode:My USB remote wake up log in...

Resolved! STM32L475RG - Having trouble jumping between multiple .bin programs in flash, program stops working.

CURRENT PRODUCT Our existing devices have a custom USB DFU bootloader starting at address 0x08000000. Our main application starts at 0x08008000, after 32Kb of space. I can jump from the main app to the bootloader with no issues (using a NVIC_Systemre...

RSikk.493 by Associate II
  • 1082 Views
  • 5 replies
  • 0 kudos

Hi, We are looking for an IoT Gateway based on STM32 MCU's, the primary reason for going with MCU's is the Low Power consumption feature of these devices, can any suggest me the suitable board/dev kit for our purpose.

As STM32F4 series can run an RTOS,RTOS like FREE RTOS is optimal to use to run multiple threads for our need, can this combination of FREE RTOS and Low Power Gateway on STM32 can be achievable in ST platform, please guide.

Resolved! Can't meet STM32G0 power spec in "Low Power sleep" mode

I had using sample code "low power sleep mode", the current measure result is over datasheet spec, how to do can get datasheet value?The measurement result is around 1mA, the datasheet show 60uA.​Hardware paltform: NUCLEO-G071RBSoftware version: 1.3....

Felix1 by Associate II
  • 784 Views
  • 2 replies
  • 0 kudos