Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I was using the CAD resources files from ST for the symbol & footprints of STM32N657B0H3Q & STM32647A0 but could find some pins missing in symbols and footprints as given in the discovery kit. So can anyone check and guide on this..I'm attaching the ...
Hello everyone, I am having a problem with a simple program. My board is a STM32-U575ZITxQ.Using only the USART1 interface, if I try to print the string: "USART1_READY" on my laptop's serial port, I have no problem. However, as soon as I also enabl...
Hi All,What is the pin pitch of each connector on STM32H747I-DISCO kit bellow. Pin pitch means the distance measured from the center of one pin to the center of the next pin.・STMod+ connector・Pmod connector・ARDUINO connectorThanks in advance.
Hello ,Does anyone use STM32F429i eval board ?The user manual (shown as the screenshot below) for my F429 eval board says it has 4 USART ,4 UART. But I can only find 1 DB9 male port marked as USART1. Also, when I use CubeIDE to configure USART1, it a...
Hi,Mouser among other sells the X-NUCLEO-67W61M1 expansion board and also provide a data brief, however the ST website seem to be void of any info on the board. Have anyone a clue to why that is?
I'm doing a project with a SD card, but I have not been able to make it work.I'm using an STM32F401RCT6 and a Micro SD Card Adapter (HW-125), I want to connect them via SPI. I've followed several tutorials online, but I haven't been able to get it to...
This question has already been asked and answered for other STM32 MCU series, but unfortunately, it didn't work for me.So, I got a brand-new STM32 Nucleo-H503RB development board to get to know it better before the project based on this MCU starts. A...
Installed STM32Cubde IDE on my machine and selected my board.I was expecting some of the pins/peripherals are set by default but as shown in the screenshot they are not.How to fix this issue please?
Hi! I have a STM32U585 board and I'm trying to make a UART loopback test. I tried two different modes:Asynchronous (Full-Duplex) - wire between the TX and RXSingle-Wire (Half-Duplex) - wire looping to itselfBoth worked in similar ways. I successfully...
I have a nucleo H743ZI board and connect to cube programmer, the programmer can only recoginze it is a H7 based MCU but not a nucleo. If i plug in a F103RB and H745ZI (both are nucleo), the programmer can see it is a nucleo board.is there any way to ...