User Activity

I am using stm32u5g7vjt6 MCU and need to program the same using STLink v2 programmer using internal power (without using external power supply). What are the modifications I need to make in configurations for the same?
While I am trying to write data in flash in memory it isn't being updated in the particular memory location while checking in debug session. And memory locations are showing 00000000 by default instead of FFFFFFFF and the image for same is attached h...
we are facing following errors during compilation:1. fatal error: cmsis_os2.h: No such file or directory OSWrappers.cpp /STM32U5G9J-DK2/Application/User/TouchGFX/target/generated line 22 C/C++ Problem2.Description Resource Path Location Typefatal err...