cancel
Showing results for 
Search instead for 
Did you mean: 

Connecting to the STM32 via an ST-LINKV/2

damien239955
Associate
Posted on November 05, 2012 at 11:30

Hello everyone,

I am currently designing an electronic board with an embedded STM32F217IG on it. I would like to interface my board with my computer through the ST-LINKV/2.

I know it is an on chip debugger but is this component also capable of simply program the STM32 or just doing debugging? It might seem a little dumb but I know some debbugger don't allow the user to flash they just allow to debug and the board stop when you unplug the debugger.

I don't know if I'm clear about what I'm asking?

Also I have another question about the connector on my board. The pin-out of the ST-LINK seems to be a classic JTAG. Am i right?

Thank you by advance for the help

Damien

#stlink #stm32f2-connection
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
frankmeyer9
Associate II
Posted on November 05, 2012 at 13:03

I know it is an on chip debugger but is this component also capable of simply program the STM32 or just doing debugging?

 

It can for sure erase/program your custom board.

Saying that, I mean with the help of some PC software, like the ST-Link Utility, or an IDE that supports the ST-Link.

Regarding to the hardware, I would take the Discovery boards as template.

Also I have another question about the connector on my board. The pin-out of the ST-LINK seems to be a classic JTAG. Am i right?

 

Not sure which ST-LINK you mean here.

The separately sold ''ST-Link'' debug adapter is capable of JTAG and SWD.

The builtin variant in the discovery boards is SWD only.

frankmeyer9
Associate II
Posted on November 05, 2012 at 13:03

<wonderful forum software crashed again...>