STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is it possible to debug STM32F0 chip with Discovery embedded ST-LINK when Vddio2 is powered by 1.8V?

Hello,I am trying to debug STM32F072 chip using ST-LINK on mb1076 Discovery board. STM32F072 is on custom board. It is powered from 3.3V except Vddio2 pin which is powered from 1.8V. I am able to program chip but when I try to debug it I get output R...

WMa�? by Associate
  • 1117 Views
  • 1 replies
  • 0 kudos

STM32L4 OTP flash programming via STLINK

Posted on August 01, 2016 at 19:03Hi,I am trying to program the OTP flash on a L4 via STLink V2, however, it gives the error: The elf loader file is not accessible.Writing 0x00000006 at 0x1FFF73F8...Error!I have tried using the CLI with the command ...

mbrejza by Associate
  • 1601 Views
  • 2 replies
  • 0 kudos

st-link v2 firmvare problem(V2.J31.S7)

after the firmware upgrade(V2.J31.S7) my st-linkv2's gives usb connection errors ST-LINK error (DEV_USB_COMM_ERR) sometimes stm32cubeProgrammer does not see the programmer at all and both cases it does not see the microcontroller. i dont have any iss...

yaksa by Associate
  • 2517 Views
  • 3 replies
  • 0 kudos