Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Posted on June 28, 2018 at 12:48Hello there,Does anyone uses the external loader of the ST-Link tool for the STM32L073xx micro-controller (MC)?What we would like to do:We have a board based on the STM32L073rz. On this board, we have an EEPROM conn...
Posted on June 25, 2018 at 13:31The stm32f4 discovery board I am using has read out protection enabled, and I can't deactivate it.First of all, it is impossible for me to set read out protection, as the attached screenshot shows, the apply button fo...
Posted on June 26, 2018 at 09:00In STM32F411 Discovery board, The STlink was not able to program the on board STM32f411, so i have usedSTLink /v2 external module to load the program into MCU. I have also applied the target voltage 3.3V to the board ...
Posted on June 25, 2018 at 18:59Hi everyone,I play with a Nucleo-F767ZI, using the ST-Link part provided on the PCB.I would like to use a ST-Link/v2 to program my MCU.I was wondering, whether it is possible to power my MCU (without USB PWR) and use ...
Posted on June 22, 2018 at 17:04I'm trying to figure out a way around this: After I program a micro, the ST Link V2 Utility keeps that .bin open as a default tab. So, on the next unit, unless you pull down the tab and browse to your new firmware, it...
Posted on June 19, 2018 at 22:47I'm trying to connect ST-Link/V2 ISOL using SWD to a STM32F030R8T6 without success using Utility. When I go to Target -> Settings, the serial number is shown. However, after pressing the Refresh button, Here's how I ...
Posted on June 18, 2018 at 09:29As I am using ios application to make tea by using tea machine which is having BLE Software and it is using STMicro Dongle. Will you please help me to update firmware version which is availabel in machine from an iOS...
Posted on June 10, 2018 at 16:13Hi, I'we got a ST-Link v2 USB dongle.The firmware on it is: V2.J17.S4Trying to upgrade the firmware to the latest V2.J30.S7I'm using the software provided by ST: ST-LinkUpgrade_007(both win subfolder and java)STM32 ...
Posted on June 02, 2017 at 02:14Hi,Today I noticed that the ST-Link on STM32F0Discovery board lost the connection with the MCU after about 10 seconds. I tried another programmer and that worked perfectly so something wrong with the Discovery board. ...
Posted on June 05, 2018 at 21:04Hi,I just got my STM32F4DISCOVERY kit (with ST-LINK/V2-A embedded). I installed TrueSTUDIO, STSW-LINK007 firmware and STSW-LINK009 USB driver. I connected the kit via mini-usb cable to the laptop, the kit starts with ...