2018-08-18 12:29 AM
after the firmware upgrade(V2.J31.S7) my st-linkv2's gives usb connection errors ST-LINK error (DEV_USB_COMM_ERR) sometimes stm32cubeProgrammer does not see the programmer at all and both cases it does not see the microcontroller. i dont have any issues in the old firmware. does anyone know where can i download the old ones?(like the version V2.J29.M18)
2018-08-18 2:58 AM
I think the ST-LINK Utilities carries J29
Will check what I have mirrored later.
2018-08-18 8:07 AM
This is v2.28.18
https://drive.google.com/open?id=0B7OY5pub_GfIM21yTDZvcmNKQUk
I will check other systems next week, but do have a selection from 2.19 to 2.31
2018-08-18 8:27 AM
The ST-LINK Utilities V4.2.0 contain V2.29.18, I can zip the update separately, but here are the utilities
https://drive.google.com/open?id=1gnmsubP8s42J5mPRYpMP20Bs_zLtAE2L