Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Dear ST community member,I am new to ST platform.I am using STM32G030C8T6 Development board from 7 Semi and ST Link V2.Dev board link: https://evelta.com/7semi-stm32g030c8t6-arm-stm32-mini-development-board/?srsltid=AfmBOorI6XBlJ_AMXNVV184OhO-lB02AFO...
Goodmorning,I am using STM32L552RCT6 in my design that I intend to use through a USB interface.I'm trying to implement the VBUS sense (compulsory since my device will be self-powered). I have read AN4879, and it's clear to me that I have to add a vol...
Dear ST Forum members,I am developing the Prototype with STM32WL microcontroller to which I provide a schematic snippet below:+ SWD 1x5 goldpin connector:If the image quality doesn't let you inspect the nets, I will provide a better image later.The 3...
I was reviewing the schematic for the STM32H7x3I-EVAL board and noticed that the ETH_nINT pin from the Ethernet PHY is connected to pin PG7 of the microcontroller.I'm having trouble finding clear documentation on how this pin functions. Could someone...
I’m designing a minimal breakout board for the STM32H757IIT6 to power it up and access a few GPIOs. The purpose is purely learning both about the STM32 dual-core system and PCB design. Since I’m a beginner, I’d like suggestions on anything essential ...
Hi,I am designing a custom board based on the STM32H753, and as part of the design process I am reviewing the MB1246 and MB1331 evaluation board schematics for reference.While studying the display interface, I noticed the following discrepancy:On the...
I am currently designing a custom board based on the STM32H753 microcontroller, and I am studying ST’s evaluation boards as reference designs for the external SDRAM interface. While comparing the schematics of MB1246 and MB1331, I noticed a discrepan...
I’m using an STM32 board to drive an SSD1322 128×64 OLED display with my own driver library. It used to work fine without issues. Without changing the code, the display suddenly became completely unresponsive. - Power supply shows 0A current draw (no...
Dear Experts,Greets,I trying to program STM32F103RCT6 micro controller using NUCLEO-F103RB evaluation board , but I am unable to debug and flash the code , i tried all the possible ways but , it didn't worked .Can somebody help me to solve this . Bes...
I try to connect by usb cable via stm32cubeprogrammer to new board but windows not see any st-link interface. older st-link v2 work fine but this on boad interfave not work. Com's led light on green and red colour. led 5VLD12 on green display work - ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.