Skip to main content
Associate III
Jan 27, 2025 12:10 PM UTC
Question

Riverdi_101 STM32H7: ST-Link can't connect to board

For more than 3 days I am trying to solve a problem of connecting to Riverdi board using external ST-link from a discovery board. I flashed apps without problem and now I can't do anything. I remember last time I was flashing an app it asked that firmware of St-link has to be updated before continuing so I proceeded. I successfully flashed the app but now I am unable to flash it again. 
 

13:07:23 : STM32CubeProgrammer API v2.18.0 | Windows-64Bits
13:07:27 : UR connection mode is defined with the HWrst reset mode
13:07:27 : ST-LINK SN : 0670FF3332584B3043153854
13:07:27 : ST-LINK FW : V2J45M31
13:07:27 : Board : STM32F4DISCOVERY
13:07:27 : Voltage : 2.91V
13:07:27 : Error: Unable to get core ID
13:07:27 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication

If I try to connect to other boards It is connected without problem.
Please help,

Regards

 

This topic has been closed for replies.

8 replies

mƎALLEm
ST Technical Moderator
Jan 27, 2025 1:11 PM UTC

Hello,

Which board? in the title you said: "STM32H7 cant connect to board"

but the log said: Board : STM32F4DISCOVERY

Could you please clarify? do you have a F4 discovery board connected via USB to your PC?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
richiAuthor
Associate III
Jan 27, 2025 1:42 PM UTC

That is the weird thing , this is the ST-link from F4 discovery board, I removed the jumpers to use only ST-link. I performed connect under Reset and performed full chip erase. However, flashing is still not possible. 

mƎALLEm
ST Technical Moderator
Jan 27, 2025 1:48 PM UTC

@richi wrote:

That is the weird thing , this is the ST-link from F4 discovery board,


Not clear. Are you using a STLINK module from F4 discovery to connect to that Riverdi board? If yes that was an important information you should provided in the first post.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.