2025-01-27 2:21 AM - last edited on 2025-01-27 3:25 AM by mƎALLEm
Hello STM Community,
I'm working on netSHIELD ethernet protocols expansion board from HilScher, In the product details they have told
| Supported Devices | STM32F4,STM32F7 |
Does it mean I can not use any other STM32 MCU with this netSHIELD industrial ethernet protocols expansion board
I want use STM32H753 because I need 9 UART and this MCU has it.
Solved! Go to Solution.
2025-01-27 3:24 AM - edited 2025-01-27 3:24 AM
Hello @moneshrathod and welcome to the community.
Only F4 and F7 products are supported but as the solution was developed by Hilscher (an ST partner) you can contact them directly over this link.
2025-01-27 2:25 AM
@moneshrathod wrote:Does it mean I can not use any other STM32 MCU with this netSHIELD industrial ethernet protocols expansion board
Almost certainly not - just that those are the MCUs for which ST provide ready-to-go examples.
2025-01-27 3:24 AM - edited 2025-01-27 3:24 AM
Hello @moneshrathod and welcome to the community.
Only F4 and F7 products are supported but as the solution was developed by Hilscher (an ST partner) you can contact them directly over this link.
2025-01-27 3:36 AM
Its still not clear. Can I use STM32H753 and put bin flash file of STM32F7 in STM32H753
2025-01-27 3:39 AM
@moneshrathod wrote:
Its still not clear. Can I use STM32H753 and put bin flash file of STM32F7 in STM32H753
No.