Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi,I am trying to develop a simple example program to control the 3 User LED's in the nucleo-144 board.Part number - STM32L4R5ZII have configured the following clock settings and BSP for the LED's.Clock Settings:/* Enable MSI oscillator and configure...
Hello.I made big board with STM32H743XI, and it works without glitch. Since STM32H747 is pin to pin compatible (TFBA240+40) I modified PCB that it will fit both processors. ( just a single ground was needed for SMPS, but i don't use it,)For some reas...
I want to send data from MCU to pc and view it on serial monitor. Is is possible to use ST-link as uart ?
Posted on February 02, 2018 at 07:30Hi, I am developing a GUI based project using Waveshare Open7xxi board. The board consists of a stm32f746 controller. Since this is a GUI project I am saving all the graphic content in external Quadspi flash. Pre...
If connected via USB 1.1 the maximum packet size should be 64. However the stlink-v3 sets the maximum packet size to 512.From dmesg: usb 2-1.3: config 1 interface 0 altsetting 0 endpoint 0x81 has invalid maxpacket 512, setting to 64
Hi,Can the STM32H7 be programmed with STLINK v2 ? ie, can it be connected to the SWD 6 pin header on the (eg: STM32F407) Discovery board, to be programmed ? Thanks,Manu
Hi,Everyone who uses ST Link under ubuntu knows the waiting time to use the ttyACM to display traces.This time is due to the ModemManager trying to send commands for a few tens of seconds.When I try to disable this service or add the STLink to the BL...
Dear, youAbout 6 month ago, I join class for ARM core.It very interesting for me.So I made customized PCB with STM32F429ZI Core.Before when I made customized PCB, I study for nucleo board.I testing my made PCB Board, I look problems.The test environm...
Hi Every one. Im noob on the linux world and im trying to use it to work in my stm32f103 (Blue pill) with my stlink and truestudio.When i plug the board and use the same hardware on Windows 10 Every thing work fine . But ok linux i have a erros "...