STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

My STLINK V2 debugger is giving "error: Target not connected" while flashing in STM32F401VBT6 controller? Please tell me the default connections of STM32F401VBT6 while flashing and debugging?

I have given 3.3V to all VDD,VDDA,VBAT,VREF+ with capacitive filtering (100 nf & 1uf) as per datasheet. BOOT0 pin is connected to GND. SWDIO and SWCLK connected to debugger pins. Still it is giving same error. when BOOT0=1, flashing is done but it gi...

ASawa by Associate II
  • 1496 Views
  • 2 replies
  • 0 kudos

ST-Link connection error

Hi,I have same probe with stm32h747i-DISCO board. I build and load image into CM4 . Then i  want load image into CM7 I have error �?ST-link connection error�?.Any idea how to fix this so ST-LINK does not throw errors and works?

IPara by Associate
  • 713 Views
  • 0 replies
  • 0 kudos