STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Host HID stm32f105

Could someone explain what exactly do I need to configure to be able to correctly use USB Host HID ?I know that I need to have external oscillator 8MHz configured, but is there anything else required?

AMaka.1 by Associate II
  • 729 Views
  • 0 replies
  • 0 kudos

STM32F103C8T6 Invalid ROM Table ST-Link

Hello,Here is my circuitBy connecting ST-Link I get "'Invalid ROM table" error. However by following this "http://www.keil.com/support/docs/3566.htm" it works fine. But I need to know why my circuit should have this option but this circuit works fine...

0690X00000BwwNXQAZ.png 0690X00000BwwPnQAJ.png
parisa by Senior
  • 3091 Views
  • 3 replies
  • 0 kudos

Pin setting of T_NRST on ST-Link

Hi, I'd like to know the pin setting of T_NRST on ST-Link.This pin setting can be set by user?What is the default setting, Push-Pull, Open-Drain, and applied any internal PU/PD resistor?Please help to advise.

FYUJI.1 by Associate II
  • 1131 Views
  • 0 replies
  • 0 kudos

CONNECTION PIN STM32F030C8

Hello everyoneI'm a novice in the industry. I need to read an STM32F030C8 mounted on a card that does not have the jtag connector and not even connector swd.However, the card has a personal 10 pin connector connected to the stm32.I need to know if th...

GDI D.11 by Associate
  • 674 Views
  • 0 replies
  • 0 kudos

I need to create a USB & Ethernet tester. The USB must be a virtual serial port and Ethernet must initiate pinging. I am using Mikroelectronica products but am having trouble. What ST products are available (Discovery board?) that can do the job?

Currently using the MikroE EasyMx Pro V7 with the STM32F407VGT6 processor. I cannot get that to work on the Ethernet side. I'd like to switch to an ST product such as the discovery board for this processor but I'm not sure if it's the right thing for...

Rick V. by Associate II
  • 3626 Views
  • 9 replies
  • 0 kudos

Touch sensing Design

Hello Friends,    I am designing a touch sensing application with method of CT acquisition principle using STM32F043k6, In that i need help to design PCB. I am confuse between hatched & full ground plane. What should i use to reduce noise immunity &...

Questions about ST-Link versions

I have, or will shortly have, three different ST-Link v2 devices. The first one us built into my Neuclo-64 for the STM32F103RB Nucleo-64 board. I know I can use the ST-Link from the Nucleo-64 board on other ST32 devices by separating it from the res...

0690X00000BxC7LQAV.png 0690X00000BxC4qQAF.png 0690X00000BxC39QAF.png
SRogers by Associate II
  • 3031 Views
  • 4 replies
  • 0 kudos