STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Upgarde Nucleo H743ZI2 to segger J-link

I have upgarded several old NUCLEO boards without any problem. All boards ware equipped with ST-LINK-V2 debugger I've tried to upgrade two new Nucleo boards board equiped wit ST-LINK-V3 .Result : Both returns error during upgrade. See attached scre...

MMagl by Associate III
  • 542 Views
  • 0 replies
  • 0 kudos

Implement ST-link design in my own boards

I successfully made a PLC board with a Nucleo development board on it.Now we are ready to ramp up production, we like to implement the Nucleo board design in our own board design.Because we make use of ST-link for drag en drop new firmware via mass-s...

WSpar.1 by Associate III
  • 1096 Views
  • 2 replies
  • 0 kudos

LAN8742 PHY does not work properly on STM32 F437VIT (Custom Boards). Everything properly wired?

Hey!I want to use the LAN8742A on a STM32F437VI.Unfortunately it doesn't work as intended. I have the suspicion that sth is not properly wired because the Ethernet LED's doesn't light up after powering up. The initialization via LWIP doesn't work pro...

0690X00000D8FCUQA3.png 0690X00000D8FPnQAN.png
MKuhl.1 by Associate II
  • 2656 Views
  • 2 replies
  • 0 kudos

St link/v2 no target connected

hiI want to know how to connect ST-LINK/V2 to STM32F030F4P6 and how to load programFor programming connecting made​st-link pin / stm pin​1 (MCU VDD)/ 3v3​4 (GND)/ GND​7 (SWDIO)/ DIO​9 (SWCLK)/ CLK​I'm using MDK keil v5Target com is SW portboard is [S...

Ppob.1 by Associate
  • 1167 Views
  • 0 replies
  • 0 kudos

STM32F746 Freeze And Debugger Lost Connection

Hello everyone,I have a custom board with STM32F746. I'm using STM32CubeIDE for this project.Board(s) working as expected. But after a while it stops working.At this point debugger connection also lost. I can not trace anything.Also ST-Link Utility ...

SCAN.1 by Associate II
  • 3303 Views
  • 10 replies
  • 0 kudos