STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Good tutorials for Nucleo-G474RE ?

Hi everyone,I a student who is new to the STM32. I've trying to find tutorials specific to the Nucleo-G474REbut I have not found any. Are there any specific tutorials to this board ? And if not what are the best tutorials out there to start learning ...

jefazo92 by Associate III
  • 2555 Views
  • 4 replies
  • 0 kudos

Resolved! ST-LINK/V2 Pins Connections

Hello,For an end of study project, I use a STM32L073RZT6 MCU.I made an STM32 / Breadboard adapter. Like that : Now, I would like to program this MCU. For this, I was given a ST-LINK / V2. I used the MCU and ST LINK datasheet to make the following con...

0693W000000TwnOQAS.jpg 0693W000000TwnYQAS.jpg 0693W000000TwnnQAC.png

How to test if a MCU is broken?

Hi all!I have developed a PCB with a stm32f4 MCU. The MCU can be programmed through SWD and works well. However, the current consumption of the whole PCB is high (~190 mA at 3.3 V). When I erase the chip, the current consumption becomes 120 mA. Could...

MCUser1 by Associate
  • 2792 Views
  • 3 replies
  • 0 kudos

why can't i update my st

I am trying to connect my stm32f103C8 via usb, when I did this I got the following message "Error in initializing ST-LINK device.Reason: (4) No device found on target".I try to update it with the stm32utility and it doesn't recognize the card.How can...

DQuir.1 by Associate II
  • 1113 Views
  • 1 replies
  • 1 kudos

About STM32G0 series and BOOT0 Pin

Hi, i have a question about this. Normally we use F0 series and BOOT0 pin must be connected to GND via 10K Ohm. So, BOOT0 pin were apart. But now, BOOT0 pin and SWCLK pin is same. I created a new schematic and I connected BOOT0/SWCLK to GND via 10K ...