STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I not to able programming the NUCLEO-H743ZI2

I have an NUCLEO-H743ZI thats works fine. So now i have buy a new NUCLEO-H743ZI2. With the samge Firmware i not able to programming the flash. I have upgrade the ST-Link V3 with the latest FW. But nothing helps. When i try to programming the Flash i ...

CDrey.1 by Associate II
  • 2868 Views
  • 5 replies
  • 0 kudos

Mounting an STWLC68 (WLCSP72 package)

Hi, I am new to working with BGA components this small. Are there any particular issues (solder paste composition, paste type, avoiding caffeine, etc.) that I should consider? I want to be able to reflow some prototype boards myself before having any...

MReev.1 by Associate
  • 670 Views
  • 0 replies
  • 0 kudos

STM32F105 USB without VBus sensing

I want to make USB which is operating in Device mode to enable pullup and pulldown resistors and reset without built-in VBus sensing pin. I've tried HAL_PCD_DevConnect(&hpcd_USB_OTG_FS) but it didn't work.How can I command USB to start working ?

STLINK-V3 support in STM32CubeIDE?

Hello,I just bought a STLINK-V3 because of its faster USB interface to speed up debugging with STM32CubeIDE. Unfortunately I cannot get it working. With some settings the target is not found with others there are errors during flash programming. Does...

Jan1 by Associate II
  • 1291 Views
  • 1 replies
  • 0 kudos

STM32L0538 Connection issues

Hello,today I've received STM32L0538 Discovery kit. The problems started right away. After connecting it to my PC via USB 3.1 port, the board gets the power, but does not work. LD1 lights up to green and LD2 to red, but LD3 and LD4 stays off, the pap...

0693W000000WAx7QAG.jpg
LLemb.1 by Associate
  • 782 Views
  • 1 replies
  • 0 kudos