Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Since STM32 STLINK Utility Command Line Interface has return codes, why STM32Cube Programmer don't have?
Hi! I have this problem with my STM32F401RE and STM32G431RB when i connect the target and try to flash my code with CubeIde, I tried to solve this using ST Link Utility, CubeProgrammer, upgrating drivers but nothings works, my G431 firmware isn't re...
Hi there, we are currently designing a sandwich board for the STM32H747i-DISCO board and we want to connect via CN8 and CN5. So far I have only found technical drawings in dm00504240.pfg (see attachment). But the exact position of the two connectors ...
I get an error pop up saying "Error in final launch sequence: and Failed to start GDB server?How do I troubleshoot this error?
Hi,I couldn't find the pcb.doc of the 32F769IDISCOVERY board. Would you please send the PCB files ?Thanks
In reading the manuals and datasheets, it seems like it should be possible to simultaneously use all 3 channels (DAC1 Channel 1, DAC1 Channel 2, and DAC2 Channel 1) of the onboard DACs at once, emitting separate values on each. However, no matter wha...
I have coded the Nucleo L476. How to mount the particular micro controller on my PCB ? What is the exact micro controller name which is there on Nucleo L476?
I think I once saw some CAD files for some of STs boards, if there are such things, where are they.
Hello,i want to program my STM32G031F4P6 chip over ST Link, but i get the error message "Can not read memory! Disable Read Out Protection and retry". Disable the Read Out Protection over the Option Bytes doesn't work. Erasing the chip also doesn't he...