Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bluenrg2 eeprom

Hi,I'm trying to interface this eeprom with Bluenrg2 http://ww1.microchip.com/downloads/en/DeviceDoc/Atmel-8828-SEEPROM-AT24CM02-Datasheet.pdfI can write correctly. I can read 1 byte at time correctly. Trying to read more than 1 bytes results in inco...

Overall impression with SPIRIT1 ISM radios ?

I have been attempting to use Silicon Labs Si443x/RFM22 ISM radio IC for over a week now with no success. My overall impression of this radio IC is poor. Lots of issues, erratas, and twitchy-spazz operation even under ideal conditions. So naturally I...

gahelton1 by Associate III
  • 729 Views
  • 1 replies
  • 0 kudos

Lora ADR in en.i-cube_lrwan v1.2.1

My project is based on the END_NODE project provided by ST.In a first time I fixed the Data rate to DR_4 for my payload need.Now i want to try to use the ADR protocol.So i change from* LoRaWAN Adaptive Data Rate * @note Please note that when ADR is ...

MMath.10 by Associate II
  • 890 Views
  • 0 replies
  • 0 kudos

BlueNRG-MS Not advertising

I have created a project for STM32L452CE using CubeMX and added BlueNRG-MS package (Additional software component).In the BlueNRG-MS package, I have selected the sensor demo application. Since our board is a custom board the pin configuration for BSP...

KS.9 by Associate II
  • 653 Views
  • 0 replies
  • 0 kudos

S2-LP Sensitivity Settings

The RSSI Threshold setting doesn't seem to lower the sensitivity of the receiver. I set the Threshold to -80dBm but the receiver still tries to receive random data out of noise with RSSIs around -110 with PQI&SQI above threshold.The rx communcation i...

0690X000006DaO4QAK.png
DKilg by Associate II
  • 925 Views
  • 0 replies
  • 1 kudos

STM32F030 (Cortex-M0) and BLE Mesh

I'd like to use STM32F030 with SPBTLE-RF. Is it possible? Can I use libBlueNRG_Mesh_CM0.a from STSW-BNRG-Mesh? STM32CubeExpansion_BLEMESH1 is available only for Cortex-M3 and M4. Is it going to be available for CM0?

grzegorz by Associate III
  • 3077 Views
  • 7 replies
  • 0 kudos