Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to start development related to BlueNRG-Mesh on Linux (Ubuntu) environment using arm-gcc open source tools?

Posted on April 18, 2018 at 08:53Hello,I've downloaded 'STSW-BNRG-Mesh' SDK from this link http://www.st.com/en/embedded-software/stsw-bnrg-mesh.html .But unfortunately, firmware SDK development is only based on Windows. I installed it on my personn...

Resolved! The Android application crashes, if I compile and run the 1.06 ver, android sample code for BLUENRG-2 SoC in my Android smartphone. What is the solution?

I am using the latest (1.06) android sample code for BLUENRG-2 SoC. After compiling the sample code with MobleLibrary-release.aar library, the apk file is created but when I am running the app in my mobile it crashes. I tried to debug the code and sa...

NKall.7 by Associate II
  • 4866 Views
  • 12 replies
  • 0 kudos

Resolved! Application Freezes when USB is connected

I am using a STM32F746NG which I am attempting to use the STM32_USB_Host_Library. I am able to initialise and start the process fine, but as soon as I connect a USB device to the port the program freezes. I am unsure if the issue is to do with the co...

AfjSpi by Associate II
  • 2612 Views
  • 5 replies
  • 0 kudos

BlueNRG-2 sleep modes questions

Hello, frens!I'm trying to make a BlueNRG-2 application that can send button state just after waking up.I use this code to manage sleep/wake states:if(!APP_FLAG(CONNECTED)) { if(on_sleep_timer == FALSE) { Timer_Restart(&t_sleep); ...

Lenoe by Associate II
  • 1832 Views
  • 2 replies
  • 0 kudos

USB Type-C SPI communication

Hi,I have a control unit that consists of a Cortex M4F, few LEDs, buttons, flash storage and LiPo battery. I also have a PCB with an accelerometer. For now, they are connected with wires and communicating through SPI. When I recharge the device (now ...

unable to wakeup bluenrg by virtual timer

hello,i am using bluenrg 1,and i write code for remote control application.Issues- I called a function to sleep bluenrg1 in main.c , and i used gpio12 and virtual timer to wake-up the device.But device is not wake-up when i put gpio12 at low unless r...

aahme.4 by Associate II
  • 786 Views
  • 0 replies
  • 0 kudos