Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to interface PCM1774 to stm32l4?

I want to interface PCM1774 DAC IC with stm32L476. PCM1774 has I2C control interface and SAI as audio data Interface. In I2C communication I am getting Ckt and data in at the end it returns device error?Can someone help me on this?

Steval-FKI433V2 doesn't work with external power supply for Nucleo and S2-LP, when the power for ST-Link doesn't supplied.

Hello.I want to decrease power consumption of Steval-FKI433V2 and to cut ST-Link PCB part, but later.Conditions:The modified program SDK_Chat.c (from S2-LP DK example) is loaded to the Nucleo uC. Uder this program Nucleo+S2-LP send back received data...

bvn123 by Associate II
  • 1116 Views
  • 1 replies
  • 0 kudos

Which files do we need from the shared sample code for BNRG Mesh, so that we can create a custom smartphone application?

I am trying to create a custom Android app taking the reference of BNRG Mesh shared sample code. I am not able to create and start the network keeping smartphone as a provisioner. I am using Android plugin version 3.2.1 and Gradle version 4.6. Please...

NKall.7 by Associate II
  • 911 Views
  • 2 replies
  • 0 kudos

320x240 lcd TFT interfacing.

I am using a TFT which support HX8238 lcd driver IC . I am confused in wire coonection between it and my main controller. If any body have its driver library please share or suggest me to making it's library.

LACTIC by Associate II
  • 738 Views
  • 0 replies
  • 0 kudos