Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG-LP can not run to main function

Recently I started to use the BlueNRG-LP,and I choosed BlueNRG345AC。I designed a PCB based on the STEVAL-IDB011V1. I try to run some example code on my design with KEIL MDK-ARM.It just totally dosn't work.the debugger is CMSIS-DAP,and I found everyti...

WYuan.1 by Associate II
  • 1176 Views
  • 1 replies
  • 0 kudos

Code samples for BLUENRG-M2SP

Hello, back in April in repsonse to a support question about developing a BLE project we were pointed to use a BLUENRG-M2SP board (along with a Nucleo-L476RG). These arrived and we were able to get the android app working where we can see the RSSI ch...

bartj1 by Associate III
  • 1537 Views
  • 1 replies
  • 0 kudos

S2-LP: CLI source code

The S2-LP DK package comes with pre-compiled binarys that are used with the GUI application(S2LP_CLI_NUCLEO_L0.hex/ bin). Is the source code available for this CLI? I want to port this to my custom board (containing a STM32G microcontroller), so I ca...

allard by Senior
  • 1771 Views
  • 2 replies
  • 2 kudos

STUSB_NVM_ReadWriteUtility_v1.01

NVM memory read/write CLI utility for STUSBxxxxDescription:Command-line interface utility to program the NVM memory of STUSBxxx products.Thanks to this tool, you can easily automate the process of flashing several devices.It requires a STM32 Nucleo b...

Resolved! BlueNRG-M2: software download and debug

Hi guys. A quick question regarding the swd and debugging on the BlueNRG-M2 module.I have made a little breakout pcb board according to the datasheet: VDD and GND are connected to 3.3V.SWD pins DIO9 and DIO10 har connected to a JLINK (Base Segger), w...

0693W00000ANHMVQA5.png
AWald.2 by Associate II
  • 1273 Views
  • 1 replies
  • 0 kudos

STEVAL-IDB005V1 and STEVAL-IDB006V1 problems

I have an STEVAL-IDB005V1 that will not enumerate as a serial port on either Windows 7 or Windows 10 so I can't use the GUI to update the Bluetooth stack. Any help would be appreciated.I also have an STEVAL-IDB006V1 that does enumerate but does not ...

RRich.3 by Associate
  • 791 Views
  • 1 replies
  • 0 kudos