Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

There are any way to establish comunication between STMF746 and the PC using the LwIP + RTOS to send and reciving data independently (without handsakeing question/anser)?

I am using the LwIP + RTOS to establish communication between STMF746 and the PC. I was able to send from STM to PC, or from the PC to STM, but I only could be able to do one thing. There are any way to program the STM to be working by 2 thread: one ...

RExpo.1 by Associate
  • 816 Views
  • 0 replies
  • 0 kudos

Resolved! BlueNRG-2 : problem with sleep state

Hello,I have a problem with the bluenrg-2. I'm using a STEVAL-IDB008V2.I measured the current while in different sleep state and here are the results :CPU-HALT : 1.6 mAWAKETIMER : 1.9 mANOTIMER : some nA.The problem is that I'm supposed to have some ...

DActi by Associate II
  • 3159 Views
  • 7 replies
  • 1 kudos

Resolved! Logs cannot be exported anymore

Started today with my STEVAL-STWINKT1B, with default firmware and an outdated version of ST BLE Sensor app.I was happy, the app connected and I was able to do a first trial, gather some data and export the data as csv by email.After that, I did an up...

SThie.1 by Associate II
  • 1658 Views
  • 2 replies
  • 0 kudos

Why does BlueNRG-1 wake up once 10 seconds?

I used BlueNRG-1 to make 1 minutes wake-up timer. But it seems wake up once 10 seconds. It causes current consumption more about 1.5uA. How to solve it? Detail information is at attach file. My code snipped is as follows. #define SCAN_RESPONSE_TIMER ...

TWu.6 by Associate II
  • 1526 Views
  • 2 replies
  • 0 kudos

BlueNRG-M2 idle power consumption too high

I am building a non-connectable beacon using a BlueNRG-M2SP board, and an STM32L412 MCU as a host, and the power consumption of the M2SP board between advertisment phases is around 24 uA, which is over 10 times higher than what the datasheet says (2....

Enter deep sleep problem of the BlueNrg-2 FreeRTOS

Please let me know below the below status and can't enter deep sleep by Bluenrg-2 FreeRTOS. ​1.vPortSuppressTicksAndSleep( TickType_t xExpectedIdleTime )2. BlueNRG_Sleep(SleepModes sleepMode, uint8_t gpioWakeBitMask, uint8_t gpioWakeLevelMask)3.ble_s...

CKim.18 by Associate II
  • 1722 Views
  • 2 replies
  • 0 kudos