Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

S2-LP (and its GUI) problems

Hi!I have S2-LP connected to S2-LP GUI (only difference - it has no EEPROM on board, so I recompiled CLI firmware with EEPROM_NO define, and it has quartz running at 25MHz). I have to receive packets with 30-50kpbs datarate, but I made slower packets...

How to read data from pins? STM32F4

Hello everyone, I would like to know how to read data from pin on STM32F4. I have a small project where I am blinking led (it's running throw Arduino board) and I would like to see throw STM32F4 when it's on and when it isn't. How should I setup pin?...

0693W000007Z0RKQA0.png
TrixCZE by Associate II
  • 2795 Views
  • 2 replies
  • 0 kudos

I am using "54VCXH163245" bidirectional level shifter in one of my ongoing projects. I am using VCCA as 3.3V and VCCB as 1.8V. My queries are: 1. Is there any power-on sequencing requirement for 1.8V and 3.3V for this device.?

However, For similar level translator device like "54AC164245", there is an explicit requirement of sequencing of 3.3V and 5.0V . Please confirm and clarify.Then datasheet of device "54VCXH163245" says VCCA must be higher or equal to VCCB, but for "...

AKuna.1 by Associate
  • 809 Views
  • 0 replies
  • 0 kudos

Make S2-LP talk to nRF905

Hello,I have a need to make the S2-LP communicate to an existing RF system which is based on the nRF905. From the reading I have done it looks like it should be possible. Does anyone have any suggestions on how to configure the S2-LP to do the job?Th...

Witek by Associate II
  • 2940 Views
  • 6 replies
  • 0 kudos