2021-02-04 2:10 PM
Hi,
I am at a complete loss, so I would really appreciate any direction you could give me.
I have bought a STEVAL-IDB011V1 evaluation board for the BlueNRG-LP and I would like to edit / extend one of the example applications. But this is my first time ever with STM MCU products. My question is then, which compiler do I have to use here? I see in the user manual of the evaluation board the Keil and IAR are mentioned, but these require a paid license. Isn't it possible to use any free of charge compiler?
EDIT: I have tried using the Atollic TrueStudio, but apparently the BlueNRG-LP is still not supported. Can somebody confirm that? Any other option, apart from that?
/Nikos
2021-02-08 4:04 PM
Use KEIL, and it is free to use for all ST Devices embedding a Cortex-M0.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.