2021-02-02 4:52 AM
Hi, I'm using Bluenrg2 chipset on a custom board and bluenrg (UART pins) is connected to the PC via USB-2-uart connection. Is this okay? What is the requirement to connect Bluenrg SW GUI with custom board without STM32
With the above mentioned connection, COM port is not getting detected
Thanks
2021-02-08 9:21 PM
Please try to flash BlueNRG-2 with DTM UART firmware,
by default under C:\Program Files (x86)\STMicroelectronics\BlueNRG-1_2 DK 3.2.1\Firmware\BLE_Examples\DTM\BlueNRG-2\DTM_UART.bin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.