Resolved! USB PD Development Environment
X-NUCLEO-DRP1M1 と NUCLE0-G071RB を持っています。USB 開発には x-cube-tcpp を使用します。ただし、構成ファイル (.ioc) を使用すると、コード生成があることに気付きました。設定ファイル(.ioc)を使用したUSBPD設定ファイル(.ioc)を使用してUSBPD用のソフトウェアを開発することはできますか?サンプルプロジェクトはありますか?
X-NUCLEO-DRP1M1 と NUCLE0-G071RB を持っています。USB 開発には x-cube-tcpp を使用します。ただし、構成ファイル (.ioc) を使用すると、コード生成があることに気付きました。設定ファイル(.ioc)を使用したUSBPD設定ファイル(.ioc)を使用してUSBPD用のソフトウェアを開発することはできますか?サンプルプロジェクトはありますか?
Hello,I have an application that uses the TCPM/TCPC architecture, with a STM32U5 acting as the port manager, and the FUSB307B as the port controller. I want to use the USB-PD middleware stack for the policy engine, however, when looking at the availa...
Hello,I am following this guide, https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Dual_Role#Clear_the_pinout, and am unable to get the device to appear in the board selection window of the UCPD monitoring soft...
Hello Sirs, I am developing a project, a portable device, which attached a 12.6 V battery pack. The device can be power on both the battery pack and a 100W PD adapter. There are a power management IC to organize and select the power path dynamically....
I am using STM32G071RB+SRC1M1 as the source and communicating with emaker in the cable, which has been enabled globally_ VCONN_ SUPPORT, but using STM32CUBEMONITOR USB TYPE-C PD to send messages to sop1 failed. Sending to sink can succeed,can
Hello,I am implementing a DRP device that is to be connected to a battery.I have this DRP example setup with the X-NUCLEO-DRP1M1 and a NUCLEO-G071RB. It is working with a 5V profile and a fixed 5V supply.I have added a 9V source PDO in CubeMX, and ca...
Hi, I am new to firmware development and using the P-NUCLEO-USB002 USB type C board for pass-through charging. I have identified the few hardware settings for the pass-through charging and data communication between USB type C Port_0 and Port_1. - co...
hi! I am using spi code off reference manual because i need make a function for write register and read the register. but with Hal not work well. i am make other function name:but, this code not work, i copy of reference manual:i don´t know how put c...
Am trying to Use of a USB to transmit data (transmit/receive) between a board and anHyperTerminal PC application. Am working with Nucleo-STM32H563 board. But i didnt get expect data in hyper terminal. Here i have attached code part . Kindly correc...
Hi,I have ported the STUSB1602 SW drivers to the Dialog/Renesas DA1469x microcontroller and would like to share my code. You can find it here:https://github.com/hupster/BLE_SDK10_examples/tree/usbpd/interfaces/usb_power_deliveryIt is based on the STM...