stm32f7508-DK Audio save in SD card example
I am using stm32f7508-DKTry to save Audio in SD card Please suggest the related example will help me to complete the task.regardssiva
I am using stm32f7508-DKTry to save Audio in SD card Please suggest the related example will help me to complete the task.regardssiva
Hey,for a project, we work with the STM32L476RG and our task is to read an audiofile from an sdcard and play it (sd/mmc interface and a class-D amplifier are provided).Does anyone have any experience with music playback on this device? Beeing fronten...
Hello,I'm getting values from an ADC an ACC, and a microphone. The ACC and ADC are in continuous acquiring mode but with different sampling rates. The microphone is turned on after a random trigger in time, basically the microphone record data for 1 ...
Hello,i read the ST instructions and looked in the EVAL Board example. There they used a audio jack via SPI but in want to play the file direct on DAC.First to check if the SD Card works i write and read a file to it (works). Then I call the "play_so...