Resolved! Why CRC is enabled in audio player example ?
why you have enabled crc for mp3 player in your examples ?What is its purpose?uint32_t Mp3Process_DecoderInit(uint8_t* pHeader, fnReadCallback_TypeDef* pReadCallback, fnSetPositionCallba...
why you have enabled crc for mp3 player in your examples ?What is its purpose?uint32_t Mp3Process_DecoderInit(uint8_t* pHeader, fnReadCallback_TypeDef* pReadCallback, fnSetPositionCallba...
i have integrated STL XCUBE class-B 2.2.0 Packages with STM32L433 controller here iam facing the test its always TEST_RUNNING not comming to Test_OK stauts, i am getting Run-time FLASH CRC Error, what could be the issue. #define ROM_START ((uint32_t...
Hi,I'm implementing the X-CUBE-STL flash test in a project on a STM32F0 device and using STM32_Programmer_CLI.exe to inject CRCs after compilations to the binary. Compilation runs without any errors/warnings. Running the flash test on the device caus...
ROM Check on STM32F030I have an STM32F030 where my product has a requirement to do a ROM check before performing any task. How can I do it? Is there any API which returns the result of ROM check done in bootloader? What’s the easiest way of achieving...