STM32 MCUs Other solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 MODBUS TCP With W5500

Hello all. I have another problem related with Modbus TCP communication. I use STM32VG board and W5500 ethernet IC. My problem is about after i establish connection, communication is broken one time in five seconds, another time in one minute. So, co...

TCP_INIT.png TCP VERİ ALMA.png TCP_VERİ GONDERME.png

STM32F405 + tlv320aic3204 - Audio Driver

Hi everyone, I hope someone can help me find or create a driver to communicate the tlv320aic3204 with the stm32f405 on my own custom board. I have been trying to replicate this tutorial (STM32 I2S ADC DMA & Double Buffering - Digital Audio Processing...

Micro SD whith micro controller

Good morning,This is my first postI' m searching for a special micro SD card with:• MCU: 32-bit (produced by ST)• MCU clock: > 100MHz• RAM: > 384 Kbytes• Flash: > 768 Kbytes• Timer function• Random number generator function• Secure memory area requir...

FuscoV by Associate
  • 205 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F103RCT6TR-CAN

Hi,          I am MURALI SELVAM I need one solution for STM32F103RCT6TR. Which is CAN pins in STM32F103RCT6TR IC. Kindly tell me. Thank you.

murali by Associate III
  • 443 Views
  • 4 replies
  • 1 kudos

Resolved! Microsecond delay for STM32G030F6P6TR

Hello I am trying to work with Microseconds delay in my codeso follow this very help full post on web POSTand I configure TIMER 3 ( I have also check with all available timer )But unfortunately, it doesn't work for my STM32GO3O MCU /* USER CODE BEGIN...

sandeep3 by Associate II
  • 1012 Views
  • 5 replies
  • 2 kudos

Can't get X-Cube-DPower to compile.

I have spent the past two days trying to get the X-Cube-DPower middleware added to an STM32CubeIDE project but it won't compile.  Does someone have a reference on how to add that to an STM32CubeIDE project?When I try to compile the code, it gives me ...

spi function in stm32l010c6t6 not work

hi! I am using spi code off reference manual because i need make a function for write register and read the register. but with Hal not work well. i am make other function name:but, this code not work, i copy of reference manual:i don´t know how put c...

spi.JPG reference manual.JPG spi2.JPG
jdo by Associate II
  • 473 Views
  • 1 replies
  • 0 kudos