User Activity

 Hello,I am using the STM32 USBPD Library in a DRP battery bank application, and want to reduce idle power consumption. In the documentation and source files, there is mention of a usbpd_lowpower.h file but I cannot find this file anywhere.There is a...
Hello,I am using the TCPP03-M20, and would like to save space/cost by combining the Source and Sink path into one mosfet gate pair.The datasheet provides an example of a combined source/sink path using two Schottky diodes and a 1M resistor with the s...
Hello,I have a custom board setup with an STM32G071GBUxN and a TCPP03-M20.I have followed this STM guide for setting it up as a DRP device.It is able to negotiate as a sink with Source only devices, and it is able to communicate over LPUART1 to show ...
Hello,I am implementing a DRP device that is to be connected to a battery.I have this DRP example setup with the X-NUCLEO-DRP1M1 and a NUCLEO-G071RB. It is working with a 5V profile and a fixed 5V supply.I have added a 9V source PDO in CubeMX, and ca...
Hello,I am following this guide, https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Dual_Role#Clear_the_pinout, and am unable to get the device to appear in the board selection window of the UCPD monitoring soft...
Kudos from