STM32 MCUs Other solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problem with dynamicaly changing USB-C PDOs

Hello,I am trying to make my own custom USB PD application on NucleoG0B1RE + SNK1M1 hardware.I want to change dynamically the SNK PDOs in my application (it should be possible according to this post). Since I want it to be working with various Source...

Marosh by Associate III
  • 890 Views
  • 6 replies
  • 6 kudos

USBC PD TCPM with FUSB307B RXSTAT alert

Hi, I've got an issue with TCPM stack running on STM32G431 with USBPDTCPM_PD3_FULL_CM4_wc32 library.The issue is related to the configuration of FUSB307B IC registers to enable SOP messages receiver at very first SOP reception. I've posted the detail...

vostrenkov_0-1714401443054.png

USB Type-C IC suggestion

Hi,I'm looking for some suggestions for the implementation of a self-powered and DRD (Dual Role Data) system provided with USB Type-C connector, but without PD support.I found two different solutions:1) Using a configuration channels protection IC (T...

VDD pin connection of STUSB1600

Hi, I am trying to use STUSB1600 as a front end interface to my USB Type-C connector and interface it with STM32L4R9 series microcontroller. It is a dual role type application but with no power delivery. Unable to understand why VDD of STUSB1600 is c...

MoniR_1-1711709267257.png MoniR_2-1711709502506.png
MoniR by Associate
  • 614 Views
  • 4 replies
  • 2 kudos

Resolved! USB Type C DRD/OTG

hi all,  i am using STM32U585 controller which is having a internal UCPD controller.my requirement is to create a module which can act as host and device using USB type C. i am taking the hardware connection as same as stm32U585 eval board(and adding...

sabari1 by Associate III
  • 1376 Views
  • 1 replies
  • 0 kudos

Resolved! UCPD + GUI Corruption message

Hello,I have a custom board setup with an STM32G071GBUxN and a TCPP03-M20.I have followed this STM guide for setting it up as a DRP device.It is able to negotiate as a sink with Source only devices, and it is able to communicate over LPUART1 to show ...

NMartin by Associate III
  • 967 Views
  • 3 replies
  • 0 kudos

Resolved! There is a problem that USBPD_CAD_Task stops

 Hello,I am developing a USB Type C chargerThe development environment is as follows HardwareNUCLEO-G071RB (tested on rev C)X-NUCLEO-DRP1M1 shield Softwarex-cube-tcppDRP1M1_DRP When this board is connected to a Windows tablet, the CAD task(USBPD_CAD_...

forst by Associate III
  • 1236 Views
  • 4 replies
  • 1 kudos

Resolved! Disable Sink and Sorce at Startup DRP1M1

  Hello,I am using the NUCLEO-G071RB and the X-NUCLEO-DRP1M1 with the X-CUBE TXPP Software Bundle.I created my project via the instructions from https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Dual_Role.Ever...

VH by Associate
  • 580 Views
  • 2 replies
  • 1 kudos