STM32 MCUs Other solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! If I want to use UCPD2 in STM32G0B1RCT6, is HSI16 the only choice as the driving clock for this integrated PD controller? May i use HSE?

In my application, UCPD2 will be active for USB type C PD Sink (45W), which will be working together with other peripherals, such as timers, USB(DEVICE), etc. If the driving clock for UCPD2 is HSI16(in datasheet described), if no other choice, that m...

0693W00000HoVNTQA3.png
Lmatt.11 by Associate III
  • 353 Views
  • 3 replies
  • 0 kudos

STM32F4 I2S clock configuration for stereo PDM

Hi guys,I have an STM32F412 discovery board and am attempting to find the best solution for connecting 8xPDM microphones in 4xStereo pairs and writing the resulting WAV to USB. The method I'm currently attempting is:Use 4xI2S peripherals, each with 2...

0690X000006CDC5QAO.jpg 0690X000006CDCKQA4.jpg
sully by Associate II
  • 511 Views
  • 2 replies
  • 0 kudos