I want to test out the usb audio device middlweare but it seem the i can't recive any audio packet, the device is configured and stall after. no isochronous transfer is done. The code is just out from cubeMX with no modification. Is there more i have...
I have two boards, STM32F303K8 and STM32F411RE, and I'm using the HAL librairie with CubeIDE 1.3.1. I don't know if these information are useful but we never know...If my question lacks information, do not hesitate to ask me what is missing in my que...
Hi, i am currently trying to make the ADC driver code for the stm32f3 version of the colorchord https://github.com/cnlohr/colorchord code work on an stm32f4, as my F4 does not have an on board microphone, also, i still want to use direct audio-line-i...