STM32 MCUs Other solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G431 USB C power delivery and Debug options

I'm designing a board G4 MCU and want to be able to power the board from USB C as well as debug or program the board.Is it possible to program the MCU via the USB C or usb 2.0 interface? If not, and I have to use SWD, what would i need in order to pr...

RMas by Associate II
  • 707 Views
  • 6 replies
  • 0 kudos

Resolved! X-CUBE-CLASSB compiler fail on IAR 9.2.0.4

Hi All,Currently I try to compiler(clean and build)  X-CUBE-CLASSB project for MCU self test function. I got error as below Does anyone know what wrong or missing setting something? I had try compiler in two project , all get error.IDE: IAR 9.20.4WI...

0693W00000NrVbkQAF.png 0693W00000NrVckQAF.png
stsan.1 by Associate II
  • 318 Views
  • 2 replies
  • 0 kudos

Application with ST self tests added throws Hard fault exception when Code optimization level is set to Medium/High(Balanced) in IAR workbench for ARM v8.22.3. Same application works for Medium/High(Balanced) optimization without ST self tests.

We are using STM32F405RG controller for our project and using ST self tests library for RAM, Flash and clock test. Currently we are trying to use code optimization option from IAR workbench functional safety version 8.22.3 and optimize code at medium...

HJosh.1 by Associate
  • 403 Views
  • 5 replies
  • 0 kudos