HI I have attached the result of the " Public Key Certificate " that I received from the SMAK application code. As a result, we are getting an Elliptic Curve Cryptography (ECC) type certificate. But as per UDAI Specification Ver 2.0 - 2022 , We...
Am trying to Use of a USB to transmit data (transmit/receive) between a board and anHyperTerminal PC application. Am working with Nucleo-STM32H563 board. But i didnt get expect data in hyper terminal. Here i have attached code part . Kindly correc...
need to transfer some string to PC via USB config. Here am implementing simple code here. But no responses in hyper terminal. Kindly help me. Am using Nucleo-STM32H563ZI board.//=======================================while (1){/* USER CODE END WHILE ...
Error in final launch sequence:Failed to execute MI command:load D:\\STUSER\\STM32CubeIDE\\workspace_1.13.0\\TEST190923\\Debug\\TEST190923.elfError message from debugger back end:Error finishing flash operation
HI. Thanks for reply.. Just i found that this code configured with Azar RTOS. Anyhow can u send particular coding part part . Task is just send / receive data via USB . ( NUCLEO-STM32H63) board. Kindly support
Hi..Am trying your way. Getting same error . Am using Nucleo-H563ZI Board Error in final launch sequence: Failed to execute MI command:load D:\\STUSER\\STM32CubeIDE\\GPIO_IOToggle\\Debug\\GPIO_IOToggle.elf Error message from debugger back end:Error f...
Hi.. Thanks for your reply. I have seen the link that you sent here. It seems helpful for me as a beginning stage. If need more information then will create a new related topic.Thanks again