Resolved! CubeMX fails to properly enable UCPD peripheral
When I enable UCPD1 in Sink mode on STM32L552 using CubeMX the clock generator tab still lists the IP as being disabled. How do I manage to get it enabled properly?
When I enable UCPD1 in Sink mode on STM32L552 using CubeMX the clock generator tab still lists the IP as being disabled. How do I manage to get it enabled properly?
Hi,I have a NUCLEO-L552ZE-Q board and I am practicing/learning the USB-C protocol. All I need is to set the voltage of USB-C to a higher voltage that the charger is capable of. The default is set to 5v.In my situation, the adapter can supply up to 12...
Hi, I'm using SAI in I2S mode to play stereo wav file. Audio Data is sent to TAS5722l which is a Mono Audio amplifier. My problem is that the FS (Frame Synchronization) signal stays always at level High. This results in a stereo audio file being play...
Hi All, I followed the updated ST tutorial on Youtube for setting up USB-PD (https://www.youtube.com/watch?v=-vsJhNIaHxE) and I can't seem to actually get it to show up on the STM32CubeMonitor-UCPD app after following as closely as I could. I am desi...
Hi,I've some trouble with the NUCLEO-L552ZE-Q using USB PD.I'm using the "USB-PD_Consumer_1port" example with STM32CubeMonitor-UCPD and can't request any power profile (see image below). I also tried different power adapters.Did I forget something?Ho...
I've a problem to setup the NUCLEO-L552ZE-Q as PD Sink.The debugger always disconnect at the following line (void HardFault_Handler(void)):CHECK_CAD_FUNCTION_CALL(USBPD_CAD_Init(USBPD_PORT_0, (USBPD_CAD_Callbacks *)&CAD_cbs, (USBPD_SettingsTypeDef *)...